To work with Kollmorgen Visualization Builder, do as follows:
Important! Be sure to use "Save" and not "Save As". The KVB is self-contained within the KAS archive and the Save As function moves the KVB out of the archive.
When you create the KVB panel with the KAS IDE, all the creation and mapping procedure is done automatically after compiling your project. So you can directly go to Design The KVB Panel.
Be aware that as soon as you change the PLC variables exported for the HMI, the mapping file must be re-imported in Kollmorgen Visualization Builder to have an up-to-date version.
Related Documents
For further information on Kollmorgen Visualization Builder, refer to the following manual:
| KVB Guide | Description | |
|---|---|---|
| Kollmorgen Visualization Builder™ Quick Start Guide |
|
Quick Start that covers the most important points to install and use Kollmorgen Visualization Builder, in order to configure HMI Panels and PCPersonal Computer operated control applications |
| Kollmorgen Visualization Builder™ User Manual |
|
Contains all the content to help you with Kollmorgen Visualization Builder |
|
Copyright © 2015 Kollmorgen™ |
|